TIDUFG5 December 2025
In the previous example, no significant RC settling time before the ADC measures Vp and Vn is assumed. In some conditions, such as the example in Figure 2-5, the time constant can be quite long. Without a workaround, the system can need to wait for a significant amount of time for the voltage to settle and thus fail to meet the standard response time requirements (for example, UL 2231-2 is 10s).
Figure 2-5 Example Waveforms With Large Time
ConstantThe time constant τ when SW1 is ON and SW2 is OFF:
There are a number of ways to address the larger time constant cases (that is, large Y caps in the µF range):