Code Composer
Studio™ (CCS) software is required to evaluate the reference design. The example code
is found in the TIDA-010985 tool folder. CCS version 12.8.1.00005 is used for this
design. When first installing CCS, be sure to check the MSP package during installation.
-
MSPM0-SDK version 2.7.0.05 is used for this design. If the SDK is not installed
from the CCS installation step, download and install the SDK. An example installation path
is: C:\ti\mspm0_sdk_2_07_00_05. Make sure that the linked resource path variables of the
project include this SDK path. Configure these settings under Project → Properties →
Resources → Linked Resources.