JAJSQ30 june 2023 BQ79616
PRODUCTION DATA
The device still supports VC channel versus CB channel by looking at the sum of (cell + bus bar measurement) comparison check on the shared channel. See Section 8.3.6.4.6.1. Additionally, bus bar measurement can be checked by comparing bus bar channel measurement from Main ADC and AUX ADC.
The BBP/N pins have built-in current sink for open wire detection. The current sink is turned on when DIAG_COMP_CTRL3[OW_SNK1:0] = 0b11. When there is a current flow through the bus bar, the (BBP–BBN) measurement is non-zero. If there is an open wire on the BBP or BBN pin, the current sink changes the (BBP–BBN) measurement to an abnormal value.