Remote temperature sensing on the TMP411-Q1 and TMP411D-Q1 devices measures small voltages using low currents, and therefore, noise at the device inputs must be minimized. Most applications using the TMP411-Q1 and TMP411D-Q1 devices have high digital content, with several clocks and logic-level transitions creating a noisy environment. The layout must adhere to the following guidelines:
- Place the TMP411-Q1 and TMP411D-Q1 devices as close to the remote junction sensor as possible.
- Route the D+ and D− traces next to each other and shield them from adjacent signals using ground guard traces, as shown in Figure 9-10. If a multilayer PCB is used, bury these traces between ground or VDD planes to shield them from extrinsic noise sources. Five-mil (0.127mm) PCB traces are recommended.
- Minimize additional thermocouple junctions caused by copper-to-solder connections. If these junctions are used, make the same number and approximate locations of copper-to-solder connections in both the D+ and D− connections to cancel any thermocouple effects.
- Use a 0.1μF local bypass capacitor directly between the V+ and GND of the TMP411-Q1 and TMP411D-Q1 devices, as shown in Figure 9-11. Minimize filter capacitance between D+ and D− to 1000pF or less for optimum measurement performance. This capacitance includes any cable capacitance between the remote temperature sensor and the TMP411-Q1 and TMP411D-Q1 devices.
- If the connection between the remote temperature sensor and the TMP411-Q1 and TMP411D-Q1 devices is less than 8 inches (20cm), use a twisted-wire pair connection. Beyond 8 inches (20cm), use a twisted, shielded pair with the shield grounded as close to the TMP411-Q1 and TMP411D-Q1 devices as possible. Leave the remote sensor connection end of the shield wire open to avoid ground loops and 60Hz pickup.