SNAA421 November 2025 LMK05318B , LMK5B12204 , LMK5B33216 , LMK5B33414 , LMK5C33216A , LMK5C33414A
If the status is undesired, run through the following debug steps.
Confirm the mux option is configured properly. For example, for Auto-Revertive, Auto Non-Revertive, and Manual Fallback modes, make sure that at least one input is assigned a priority through the DPLLx_REFy_AUTO_PRTY register.
Try forcing a selection by manually selecting one input using the Manual Holdover mode. Make sure to specify the selected input through either register or pin setting. If the DPLL remains in Holdover even though the reference is valid, contact TI by posting on the public TI E2E forum for further assistance.
The DPLL input registers can be incorrect. Try generating a new configuration using TICS Pro.