SNAA421 November 2025 LMK05318B , LMK5B12204 , LMK5B33216 , LMK5B33414 , LMK5C33216A , LMK5C33414A
If the status is undesired, run through the following debug steps.
Confirm the APLL is configured properly and can achieve lock by disabling the DPLL. If the DPLL is enabled, the DPLL can rail the APLL which can cause the frequency to unlock and make the debug more complicated. Re-enable the DPLL once APLL lock is validated.
Each APLL VCO must be calibrated to achieve APLL lock and deliver the best phase noise performance. The VCO calibration establishes the best operating point within the VCO tuning range. After POR, hardware reset, or software reset, the VCO calibration is executed automatically. The APLL reference must be stable and considered valid before the start of calibration to provide a successful calibration and APLL lock. The output drivers are held in a muted state until the VCO calibration completes and the APLL locks. If you are not getting an APLL lock, try issuing a software reset after loading the register configuration. The best practice is to recalibrate the VCO whenever the PFD, charge pump, APLL loop filter, or APLL N divider registers are modified.
The PFD has two inputs: the APLL R divider path (from the XO input) and the APLL N divider path (from the VCO), as shown in Figure 2-2. The GPIO pins of the LMK devices can be configured as "APLL R divided by 2" and "APLL N divided by 2" signals which applies a divide by 2 to each path to reduce the GPIO output frequency. Configure the two GPIO pins per Table 2-12 and Table 2-27. Note that the APLL R divider is unavailable when R=1 (bypassed); in this case, probe the external APLL reference. Probe the two signals using an oscilliscope. Confirm that the two signals are present, have the same frequency, and are frequency-locked to each other. During a locked APLL state, the two signals are triggered to each other with no drifting observed on the oscilliscope.
| DEVICE FAMILY | TICS PRO FIELD NAME | PIN NAME | APLL R DIVIDED BY 2 REGISTER SETTING | ||
|---|---|---|---|---|---|
| BAW APLL | APLL2 | APLL1(2) | |||
| LMK05318B, LMK05318 | PLLx R Divider, div-by-2 | STATUS0 | N/A(1) | R48[6:0] = 0x0F | N/A |
| STATUS1 | N/A(1) | R49[6:0] = 0x0F | N/A | ||
| LMK5B or LMK5CA | PLLx R-Divider Divided By 2 | Required for any GPIOx | R70[0] = 1 R872[3] = 1 | R70[0] = 1 R808[3] = 1 | R70[0] = 1 R736[3] = 1 |
| GPIO0 | R57[6:0] = 0x55 | R57[6:0] = 0x54 | R57[6:0] = 0x53 | ||
| GPIO1 | R58[6:0] = 0x55 | R58[6:0] = 0x54 | R58[6:0] = 0x53 | ||
| GPIO2 | R59[6:0] = 0x55 | R59[6:0] = 0x54 | R59[6:0] = 0x53 | ||
| DEVICE FAMILY | TICS PRO FIELD NAME | PIN NAME | APLL N DIVIDED BY 2 REGISTER SETTING | ||
|---|---|---|---|---|---|
| BAW APLL | APLL2 | APLL1(1) | |||
| LMK05318B, LMK05318 | PLLx N Divider, div-by-2 | STATUS0 | R48[6:0] = 0x05 | R48[6:0] = 0x08 | N/A |
| STATUS1 | R48[6:0] = 0x05 | R49[6:0] = 0x08 | N/A | ||
| LMK5B or LMK5CA | PLLx N-Divider, Divided By 2 | Required for any GPIOx | R70[0] = 1 R872[3] = 1 | R70[0] = 1 R808[3] = 1 | R70[0] = 1 R736[3] = 1 |
| GPIO0 | R57[6:0] = 0x52 | R57[6:0] = 0x51 | R57[6:0] = 0x50 | ||
| GPIO1 | R58[6:0] = 0x52 | R58[6:0] = 0x51 | R58[6:0] = 0x50 | ||
| GPIO2 | R59[6:0] = 0x52 | R59[6:0] = 0x51 | R59[6:0] = 0x50 | ||
Try using the charge pump register settings provided by the Default Configuration tab in TICS Pro Software. Too much charge pump current can oversaturate the APLL resulting in unstable APLL outputs. Too little charge pump current can cause the APLL to unlock and become an open-loop.
Try using the loop filter register settings provided by the Default Configuration tab in TICS Pro Software. Additionally, confirm the external capacitor applied to the LFx pin is per data sheet recommendation. The external capacitor is the "C2" for the respective APLLx loop filter.
Measure the voltage of the LFx pin over time to observe the trend. During normal operation, the voltage varies over time due to variation in the APLL reference frequency (when the APLL is locked), DPLL reference frequency (when the DPLL is locked), and temperature. The typical tuning voltage is somewhere in the middle. Too low or too high can mean the APLL has railed to an incorrect frequency. If the DPLL is enabled, the tuning voltage can be railed (< 0.1V or > 2.4V) because the DPLL drives the APLL to rail off. A reading of 0V is not expected behavior and can be due to a damaged or improperly soldered device. If the voltage is not changing, but is not 0V, contact TI by posting on the public TI E2E forum for further assistance.