SPRADB7 September 2023 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2-Q1 , AM263P4 , AM263P4-Q1 , AM2732 , AM2732-Q1
The design of a PCB will have a strong correlation to the difference between junction and ambient temperature. The ideal goal is for the junction temperature to be as close as possible to the ambient temperature but when the heat is not able to efficiently diffuse away from the SoC, then the delta between junction and ambient temperature will be larger. The thermal resistance between the board and ambient temperature can be broken up into four separate thermal resistances that will have varying values based on the system design:
Figure 2-4 Breakdown of RΘBAIt is easy to imagine how some simple design choices can help with decreasing the RΘBA which subsequently decreases the RΘJA. A few examples of design choices to help with thermal performance are increasing copper volume of thermal vias, adding additional copper layers, or increasing board size. For a fullbreak down of design choices that affect thermal performance, refer to Section 3.