SPRADB7 September 2023 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM2732 , AM2732-Q1
The thermal design of a PCB can impact various aspects of a design:
Factor | Description |
---|---|
Functionality/Reliability | Will the system work in the expected temperature range? |
Cost | Will changes for thermal considerations make the board cost too much? |
Weight | Is there a weight restriction that would limit thermal dissipation options? |
User experience | Will the user burn themselves if they touch the board during operation? |