SPRADB7 September 2023 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM2732 , AM2732-Q1
Similar to how narrowing a water pipe will bottleneck the flow of water, traces and via cutouts can lead to bottlenecking of the thermal dissipation. Each ground layer on the board should be reviewed to make sure that there are no breaks in the thermal pathing. Multiple vias together in a line or array can create a cutout on the ground layer that will negatively impact the thermal flow away from the SoC.
For best thermal performance: