SPRUIY2A November 2024 – March 2025 F29H850TU , F29H859TU-Q1
The CALL.PROT operation is permitted to cross STACKs. When arriving at the destination address of the CALL.PROT, the ENTRY1.PROT and ENTRY2.PROT instructions must be the first instructions executed. If these instructions are not present, the CPU enters the FAULT state. Upon returning from the CALL.PROT operation, the very first instruction at the return address must be the EXIT.PROT instruction. If the EXIT.PROT instruction is not present, the CPU enters the FAULT state. These ENTRY and EXIT instructions control the entry and exit points of the code when security boundaries are crossed and enable user code to check any passed parameters or data before being used.