SPRUIY2A November 2024 – March 2025 F29H850TU , F29H859TU-Q1
NMIs cannot be masked or blocked in the CPU. There is no global enable/disable bit for the NMI line in the CPU. Because of this, any interrupts that are received on the NMI line are directly passed to the CPU for prioritization. Priority is then decided amongst the interrupt types (NMI, RTINT, and INT lines). NMI always has highest priority and asserts within any RTINT or INT currently executing. ATOMIC instructions in RTINT or INT ISRs cannot block or prevent NMI from asserting. ATOMIC instructions have no effect on NMI.