SPRUIY2A November 2024 – March 2025 F29H850TU , F29H859TU-Q1
Unlike the NMI or RTINT interrupt lines, the INT line uses the standard software stack for context save and restore. Only one of the multiple available CPU stacks can be used for INT. This is configured by the INTSP register in the external PIPE module. If an INT vector points to the wrong LINK which is associated with a different STACK (security-assigned stack), then an NMI fault is generated.
If the current stack pointer is not pointing to the INTSP, then any pending INT remains pending until the stack pointer points to the selected INTSP stack.