DLPU018I October 2014 – November 2023 DLPC900
The DLPC900 only supports long axis image flip for single controller DMDs. This command is not supported when combined with a dual controller DMD.
The Long-Axis Image Flip defines whether the input image is flipped across the long axis of the DMD. If this parameter is changed while displaying a still image, then re-send the still image. If the image is not re-sent, the output image might be slightly corrupted. Figure 2-1 shows an example of a long-axis image flip. In Structured Light mode, the image flip takes effect on the next bit-plane, image, or video frame load.
I2C | USB | |
---|---|---|
Read | Write | 0x1008 |
0x08 | 0x88 |
BYTE | BITS | DESCRIPTION | RESET | TYPE |
---|---|---|---|---|
0 | 0 | Flips image along the long side of the DMD: | d0 | wr |
0 = Disable flip | ||||
1 = Enable flip | ||||
7:1 | Reserved | d0 | r |