DLPU018I October 2014 – November 2023 DLPC900
The Start Address command serves three purposes.
1) Specifies the start address of the flash download write operation. It is the responsibility of the user to ensure that the start address is on a sector boundary in the current flash device.
2) Specifies the start address where checksum operation begins.
3) Specifies the sector address to be erased. The address must be the start of a sector.
The Flash Data Size command always follows 1 and 2 above, which defines how many bytes to be downloaded or how many bytes to include for the checksum operation.
The user must avoid erasing the first 128 kilobytes of the boot flash as this contains the boot image. Please see Table 2-17 for a definition of areas that must not be erased.
I2C | USB |
---|---|
Write | 0x0032 |
0x32 |
BYTE | BITS | DESCRIPTION | RESET | TYPE |
---|---|---|---|---|
3:0 | 31:0 | 4 byte flash address. Byte 0 is LSB, byte 4 is MSB. Valid Range:
| 0x0 | w |