SBASB61 August 2026 ADS114S18 , ADS124S18
PRODUCTION DATA
The SPI_CRC_FAULTn flag indicates if a SPI CRC fault occurred on SDI in the previous SPI frame. The execution of the command in the frame where the SPI CRC fault occurred is blocked. Instead, a no operation command is executed. Commands in following frames are not blocked. The SPI_CRC_FAULTn bit updates in every new SPI frame based on the CRC result of the previous SPI frame. Enable the SPI CRC using the SPI_CRC_EN bit. In addition, enable the transmission of the STATUS header using the STATUS_EN bit to get notified about any SPI CRC faults. See the SPI CRC section for details about the SPI CRC implementation.