SBASB61 August 2026 ADS114S18 , ADS124S18
PRODUCTION DATA
To help detect potential sensor faults, the ADS1x4S1x provide a pair of programmable burn-out current sources (BOCS). Use the STEPx_BOCS[1:0] bits to enable the current sources and to set the values to 0.2μA, 1μA, or 10μA.
The BOCS connect to the PGA inputs after the internal multiplexer. When enabled, one BOCS sources current from AVDD to the selected positive analog input (AINP) and the other BOCS sinks current from the selected negative analog input (AINN) to AVSS.
In case of an open-circuit in the external sensor or a sensor wire disconnection, these BOCS pull the positive input toward AVDD and the negative input toward AVSS, resulting in a full-scale reading. A full-scale reading can also indicate that the sensor is overloaded or that the reference voltage is absent.
A near-zero reading can indicate a shorted sensor. Distinguishing a shorted sensor condition from a normal reading can be difficult, especially if an RC filter is used at the inputs. The current sources create a voltage drop across the external filter resistors and the residual resistance of the internal multiplexer. That means, even when the sensor is shorted, a small voltage is present at the PGA inputs and the ADC consequently outputs a voltage larger than zero. The residual resistance of the internal multiplexer typically ranges from about 400Ω at AVDD = 3.3V to 1.6kΩ at AVDD = 1.8V.
The ADC readings of a functional sensor can be corrupted when the burn-out current sources are enabled. Therefore, disable the burn-out current sources when performing precision measurements, and only enable the BOCS to test for sensor fault conditions during a dedicated diagnostic measurement.
Disable the BOCS when using global-chop mode (GC_EN = 1b). The burn-out current source function is not compatible with global-chop mode.
The burn-out current sources remain active in idle mode, but turn off in standby and power-down mode.