SBASB61 August 2026 ADS114S18 , ADS124S18
PRODUCTION DATA
In 3-wire SPI mode, an unintended SCLK can misalign the frame, resulting in loss of frame synchronization to the host. As shown in Figure 7-40, the SPI is resynchronized without requiring a device reset by sending an SPI re-align pattern. The re-align pattern is a minimum of 63 consecutive 1s followed by one 0 at the 64th SCLK. The 65th SCLK starts a new SPI frame. The device also accepts a re-align pattern with more than 63 consecutive 1s followed by one 0. In that case, the new frame starts with the SCLK rising edge following the 0. Optionally, the ADC can be completely reset by toggling the RESET pin or by using the reset pattern shown in the Reset by SPI Input Pattern section.