SBASB61 August 2026 ADS114S18 , ADS124S18
PRODUCTION DATA
Configure the sequencer operation and behavior using the various bits summarized in Table 7-20. For more details see the respective bit field descriptions in the Register Map section.
| REGISTER BITS(1) | DESCRIPTION |
|---|---|
| Status and General Configuration Page | |
| STEP_INIT[4:0] | This pointer determines the step page configuration that is used for the first conversion when the sequencer starts. In idle or standby mode, this pointer selects the active step page configuration, irrespective if the page is enabled or disabled by the respective STEP_x_EN bit. |
| SEQ_MODE[1:0] | Selects the sequencer operation as described in the Sequencer Mode section. |
| STOP_BEHAVIOR[1:0] | Determines how the sequencer stops when the host requests to stop the sequencer. |
| STEP_x_EN | The individual enable bits select a step to be included within the sequence when SEQ_MODE[1:0] = 10b or 11b. These bits are ignored when SEQ_MODE[1:0] = 00b or 01b. |
| Step x Configuration Pages | |
| STEPx_NUM_CONV[4:0] | Determines how many consecutive conversions the sequencer executes on the respective sequence step. The digital filter does not reset between those consecutive conversions of a step. These bits are ignored when SEQ_MODE[1:0] = 01b. |
| STEPx_DELAY[6:0] | Determines how long the sequencer waits after selecting a step configuration page before starting conversions. This is to allow for any settling of the selected measurement signal. The digital filter is held in reset during this delay time. |
See the Register Map section for details on how to access the various register pages for configuration. Section Device Initialization and Starting the Sequencer shows an example of how to configure the sequencer.
Do not change any register settings on the individual step configuration pages while the sequencer is active. Any write operation to any of the step configuration pages stops the sequencer immediately.