The main ADC clock signal (CLK) generates the ADS1285 modulator clock (fMOD) in one of two ways:
- A crystal oscillator and the accompanying clock dividers can provide a selectable frequency for the entire range of the ADC.
- The onboard crystal oscillator (Y1) provides the nominal 8.192MHz clock frequency (default)
- The dividers (U6) step down the frequency to 4.096MHz
- J8 allows the user to select between these frequencies and connect them directly to CLK by using a shunt
- Provide an external main clock to a subminiature version A (SMA) connector (J5) or to pins 4 or 2 of J7 when a shunt does not select the frequency from the crystal oscillator.
- In this case, a shunt must not cover J7 so that CLK is connected to any of the crystal oscillator signals
- Be sure to review the valid CLKIN input frequency in the data sheet
Note: All clock sources are sourced back to the PHI connector (J6) so that SCLK is synchronous to CLK.
Figure 2-6 shows a schematic for the clock source.