SLAAEF9A November 2023 – May 2025 MSPM0C1104 , MSPM0G3507 , MSPM0H3216 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1306 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Launch a new workspace. The workspace means the address where to copy the imported project. The step in CCS is same as that in e2studio.
Figure 2-20 CCS Launch WorkspaceTo create a new project, go to file--> new-->CCS project. There are two important items that need to be done. The first one is to choose MSPM0 device and the other one is to choose the connection, as shown in Figure 2-21. And then, the program can be created after project name is added and press finish button.
This is similar to the creation of new project in e2studio , which requires selecting device, tool chain, and program name.
TI recommends to find the MSPM0 SDK example, which introduces how to use CCS in Section 2.2.4.
Figure 2-21 Create a New Project in CCSFigure 2-22 shows a quick introduction to CCS functions.
Figure 2-22 Commonly Used FunctionsDebug functions:
Figure 2-23 Commonly Used Debug FunctionsProject properties common used settings:
Figure 2-24 Commonly Used Project SettingsFor detailed information, refer to Code Composer Studio IDE Version 12.4+ for MSPM0 MCUs — Code Composer Studio IDE for MSPM0 MCUs 1.0 documentation.