SLAAEF9A November 2023 – May 2025 MSPM0C1104 , MSPM0G1218 , MSPM0G3218-Q1 , MSPM0G3507 , MSPM0H3215 , MSPM0H3216 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1306 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The file content is shown in the SDK folder after the content is finished downloading. The file location is c:/ti/mspm0_sdk_xxx by default as shown in Figure 2-27. This location contains the mostly used folders are examples folder and docs folder.
Figure 2-27 MSPM0 SDK FoldTable 2-6 shows a summary of example coverage.
| Supported by SDK | Platform | ||||
|---|---|---|---|---|---|
| IDE | CCS | Keil | IAR | ||
| Compilers | TI Arm-Clang | GUN Arm | Arm or Keil Compiler | IAR Arm compiler | |
| RTOS | FreeRTOS | ||||
| Code examples | Driverlib TI Drivers (drivers) | ||||
Three empty projects in the nortos examples are available for users to build a project. Table 2-7 the differences.
| Example | Use Sysconfig | Include Library Files Into Project |
|---|---|---|
| empty | Yes | No |
| empty_library | No | Yes |
| empty_driverlib_src (Suggested) | Yes | Yes |
As for the docs folder, the structure and the important documents are shown in Figure 2-28.
Figure 2-28 Document Overview