SLLSFR8B September 2025 – January 2026 TCAN5102-Q1
ADVANCE INFORMATION
PWM0_IR is shown in Figure 7-124 and described in Table 7-165.
Return to the Summary Table.
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RSVD | PULSE_OVF | IAS | RC | ||||
| R-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7-3 | RSVD | R | 0h | Reserved |
| 2 | PULSE_OVF | R/W1C | 0h | Current Pulse Overflow Set when the CUR_PULSE counter overflows
|
| 1 | IAS | R/W1C | 0h | Input Auto Stop Interrupt Sets when the input auto stop condition has occurred, if the PWM is configured to immediately stop, then the output will also be stopped (reflected by the RC bit). If PWM is configured to begin the stop ramp on an IAS triggere, then then this interrupt is set immediately when the input condition happens and the RC bit will be set when the output turns off.
|
| 0 | RC | R/W1C | 0h | PWM Ramp Complete Sets when the ramp has finished.If AS_EN = 1 (auto stop), then this happens when the PWM channel turns off. If AS_EN = 0, then this gets set when the PWM has reached the end value. If IAS_EN = 1 (input auto stop), then this will get set once the PWM output is stopped If a stop ramp is manually activated, the RC bit will be set once the ramp completes and the output is turned off. Note: If an on-ramp is in progress and a stop condition occurs, the RC bit will NOT be set for the on-ramp, but only once the output stops due to the stop condition
|