SLLSFR8B September 2025 – January 2026 TCAN5102-Q1
ADVANCE INFORMATION
In addition to supporting up or down ramps, the TCAN5102-Q1 also supports the ability to do an entire acceleration and deceleration ramp with only a "start" signal from the upstream controller. This is set up by setting a counter that counts the number of pulses, and is used to determine when to begin the "stop/off" ramp. There is also another counter for the maximum number of pulses allowed. This acts as a hard cut off for stopping PWM output when a total number of pulses have been generated during a PWM ramp. The stop feature is supported in all PWM modes (duty cycle, frequency, or static).
A user-selectable GPIO can be used to trigger a stop ramp or an immediate off condition. This is useful for a limit switch, or some sort of fault to immediately disable the PWM output.