SLLSFZ8 November 2025 MCF8329HS-Q1
PRODUCTION DATA
An 8-bit CCIT polynomial (x8 + x2+ x + 1) is used for CRC computation.
CRC Calculation in Write Operation: When the external MCU writes to MCF8329HS-Q1, if the CRC is enabled, the external MCU has to compute an 8-bit CRC byte and add the CRC byte at the end of the data. MCF8329HS-Q1 computes CRC using the same polynomial internally and if there is a mismatch, the write request is discarded. Input data for CRC calculation by external MCU for write operation are listed below:
CRC Calculation in Read Operation: When the external MCU reads from MCF8329HS-Q1, if the CRC is enabled, MCF8329HS-Q1 sends the CRC byte at the end of the data. The CRC computation in read operation involves the start byte, control words sent by external MCU along with data bytes sent by MCF8329HS-Q1. Input data for CRC calculation by external MCU to verify the data sent by MCF8329HS-Q1 are listed below :