SNVSCO1 November 2025 LM5126A-Q1
PRODUCTION DATA
Monitor the average VI input current at the IMON-pin. The average sensed input current is generating a source current at the IMON-pin, which is converted to a voltage by the resistor RIMON. The resulting voltage VIMON is calculated according to Equation 17, the required resistor RIMON according to Equation 16. VIMON regulates up to 3V and is self protecting not reaching the absolute maximum value.
RSNS is the sense resistor. IIN is the input current, GIMON the transconductance gain and IOFFSET the offset current given in the electrical characteristics table.
Limit the average input current by choosing an appropriate resistor connected to the ILIM-pin. When the input current limit is active, VOUT is regulated down until the set average input current limit is reached. In case VOUT is regulated below the VI voltage the current cannot be limited anymore. The DLY-pin capacitor CDLY adds an additional delay time tDLY to activate and deactivate the average input current limit (see Average Current Limit). When the ILIM-pin voltage reaches the threshold VILIM (typical 1V) the source current IDLY is activated charging up the DLY-pin capacitor CDLY. The DLY-pin voltage VDLY rises until VDLY_peak_rise is reached, which activates the average input current limit. The ILIM-pin voltage is regulated to VILIM and the input current is regulated down to the average input current limit set by RILIM resulting in a VOUT drop. To exit the avarage current limit regulation the output load has to decrease, which causes VOUT to rise and VILIM to fall below VILIM_reset (typical 0.88V). VILIM_reset activates the sink current IDLY, which discharges the DLY-pin capacitor CDLY. When VDLY reaches VDLY_peak_fall the average input current limit is deactivated and the DLY-pin is discharged to VDLY_valley. The required resistor RILIM is calculated according to Equation 18, the capacitor CDLY according to Equation 20.
While a constant delay is added by the DLY-pin capacitor a VOUT load dependent delay can be added by adding a RC tank to the ILIM/IMON-pin in parallel to the RILIM resistor. The RC tank resistor RC_IMON is calculated according to Equation 73 and the capacitor CIMON according to Equation 72.