SNVSCS7D April 2025 – November 2025 TPSM33606-Q1 , TPSM33610-Q1 , TPSM33620-Q1
PRODUCTION DATA
With a steady-state input voltage range from 3V to 36V, the TPSM336xx-Q1 device is intended for step-down conversions from typical 12V to 36V input supply rails, as example. The schematic circuit in Figure 7-1 shows all the necessary components to implement a TPSM336xx-Q1-based buck regulator using a single input supply.
Take extra care to confirm that the voltage at the VIN pin does not exceed the absolute maximum voltage rating of 40V during line or load transient events. Voltage ringing at the VIN pins that exceeds the absolute maximum ratings can damage the IC.