SNVSCS7D April 2025 – November 2025 TPSM33606-Q1 , TPSM33610-Q1 , TPSM33620-Q1
PRODUCTION DATA
In some cases, an input UVLO level different than that provided internal to the device is needed. This need can be accomplished by using the circuit shown in Section 7.3.3. The input voltage at which the device turns on is designated as VON while the turn-off voltage is VOFF. First, a value for RENB is chosen in the range of 10kΩ to 100kΩ, then use Equation 4 to calculate RENT and Equation 5 to calculate VOFF.
Figure 7-6 Setup for
External UVLO Applicationwhere
Refer to the Electrical Characteristics table for other terms.