SPRAC76H November   2022  – October 2025 AM5706 , AM5708 , AM5716 , AM5718 , AM5726 , AM5728 , AM5729 , AM5746 , AM5748 , AM5749 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62L , AM62P , AM62P-Q1 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , AM6526 , AM6528 , AM6546 , AM6548

 

  1.   1
  2.   Sitara Processor Power Distribution Networks: Implementation and Analysis
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Acronyms Used in This Document
  5. 2Guidelines for PCB Stack-Up
  6. 3Physical Layout Optimization of the PDN
  7. 4Static PDN Analysis (IR Drop Optimization)
  8. 5Dynamic Analysis of PCB PDN
    1. 5.1 Selecting Decoupling Capacitors to Meet ZTARGET
  9. 6Checklist for PDN
  10. 7Implementation Examples and PDN Targets
    1. 7.1  AM570x
    2. 7.2  AM571x
    3. 7.3  AM572x
    4. 7.4  AM574x
    5. 7.5  AM65xx/DRA80xM
    6. 7.6  AM62xx
    7. 7.7  AM64xx
    8. 7.8  AM62Ax
    9. 7.9  AM62Px
    10. 7.10 AM62Lx
  11. 8Revision History

Guidelines for PCB Stack-Up

The PCB stack-up (or layer assignment) is an important factor in ensuring optimal performance of a power distribution scheme. An optimized PCB stack-up for improved power integrity performance can be achieved by following these recommendations:

  • Power and ground plane pairs/”islands” should be closely coupled together. The capacitance formed between the planes can be used to decouple the power supply. Whenever possible the power and ground planes should be solid to provide a continuous return path for return current.
  • Use a thin dielectric between the power and ground plane pair. Capacitance is inversely proportional to the separation of the plane pair so minimizing the separation distance (the dielectric thickness) will help to maximize the capacitance.
  • Keep the power and ground plane pair as close to the PCB top and bottom surfaces as possible (see Figure 2-1). This will help to minimize the associated loop inductance of the decoupling capacitors, vias, and the power/ground plane pair spreading loop inductance.
 Minimize Loop Inductance by
                    Optimizing Layer Assignments in the PCB Figure 2-1 Minimize Loop Inductance by Optimizing Layer Assignments in the PCB

The placement of power and ground planes in the PCB stack-up (determined by layer assignment) has a significant impact on the parasitic inductance of the power current path as shown above. For this reason, it is recommended to consider layer order in the early stages of the PCB PDN design cycle, putting high priority supplies in the top half of the stack-up and low-priority supplies in the bottom half of the stack-up as shown in the examples below. Figure 2-2 and Figure 2-3 show examples of typical PCB stack-ups designed with power distribution performance in mind. Device-specific stack-up examples can be found in Section 8.

 Example Stack-Up Utilizing
                    High-Density Interconnect Vias Figure 2-2 Example Stack-Up Utilizing High-Density Interconnect Vias
 Example Stack-Up Utilizing
                    Plated-Through-Hole (PTH) Vias Figure 2-3 Example Stack-Up Utilizing Plated-Through-Hole (PTH) Vias