SPRAC76H November 2022 – October 2025 AM5706 , AM5708 , AM5716 , AM5718 , AM5726 , AM5728 , AM5729 , AM5746 , AM5748 , AM5749 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62L , AM62P , AM62P-Q1 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , AM6526 , AM6528 , AM6546 , AM6548
The following are important requirements that need to be implemented in the PCB PDN design:
Figure 3-1 Characteristics of a “Real” Capacitor With ESL and ESRThe magnitude of the impedance of this series model is given in Equation 1.

Figure 3-2 shows the resonant frequency response of a typical capacitor with self-resonant frequency of 55 MHz. The impedance of the capacitor is a combination of its series resistance and reactive capacitance and inductance as shown per Equation 1.
Figure 3-2 Typical Impedance Profile of a Capacitor
Figure 3-3 Example of “Co-Planar’ Shielding of Power Net Using Ground Guard-BandAs the capacitors have both series inductance and resistance that will impact their effectiveness, it is critical that the following recommendations are adopted in placing them on the power distribution network. Whenever possible make sure to mount the capacitor with the geometry that will minimize the mounting inductance and resistance. The capacitor mounting inductance and resistance includes the inductance and resistance of the pads, the trace, and the associated vias.
The length of a trace used to connect a capacitor has a significant impact on the parasitic inductance and resistance of the mounting. This trace should be as short and wide as possible. Wherever possible, minimize the trace by locating vias near the solder pad landing. Further improvements can be made to the mounting by placing vias to the side of capacitor lands or by doubling the number of vias. If the PCB manufacturing process allows, and if cost-effective, via-in-pad (VIP) geometries are strongly recommended.
The most common via placement geometries are proved below, in order of preference for reducing parasitic impact:
Figure 3-4 Capacitor Mounting GeometriesIn addition to mounting inductance and resistance associated with placing a capacitor on the PCB, the effectiveness of a decoupling capacitor also depends on the spreading inductance and resistance that the capacitor sees with respect to the load. The spreading inductance and resistance is strongly dependent on the layer assignment in the PCB stack-up (see Figure 2-1).