SPRAD28 October 2022 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM26C31 , AM26C31-EP , AM26C31C , AM26C31I , AM26C31M , AM26C32 , AM26C32-EP , AM26C32C , AM26C32M , AM26LS31 , AM26LS31M , AM26LS32A , AM26LS32AC , AM26LS32AM , AM26LS33A , AM26LS33A-SP , AM26LS33AM , AM26LV31 , AM26LV31E , AM26LV31E-EP , AM26LV32 , AM26LV32E , AM26LV32E-EP , AM2732 , AM2732-Q1
There are few methods to debug the stack. One of them is using the stack peak of the ROV (described in detailed in the ROV section). Another method that can be useful is to set a watchpoint to the end of stack, as described in the Watchpoints section. In addition, the compiler provides stack protection functionality in the form of the following options. To be able to use them, enable those "flags" in Project → Properties → Build → Arm Compiler → Edit flags.