SPRAD28 October 2022 AM2431 , AM2432 , AM2434 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM26C31 , AM26C31-EP , AM26C31C , AM26C31I , AM26C31M , AM26C32 , AM26C32-EP , AM26C32C , AM26C32M , AM26LS31 , AM26LS31M , AM26LS32A , AM26LS32AC , AM26LS32AM , AM26LS33A , AM26LS33A-SP , AM26LS33AM , AM26LV31 , AM26LV31E , AM26LV31E-EP , AM26LV32 , AM26LV32E , AM26LV32E-EP , AM26S10 , AM2732 , AM2732-Q1
Include the below file to access the APIs:
#include <stdio.h>
#include <kernel/dpl/DebugP.h>
Example usage for assert:
void *addr = NULL
/* This will assert when address is NULL */
DebugP_assert(addr!=NULL);
Example
usage for
logs:Uint32_t value = 10;
char *str = "Sitara AM2x debugging";
/* Use snprintf to format the string and then call logging function */
DebugP_log("This is %s and value is = %d", str, value);
Example
usage for
scanf:DebugP_log("Enter a 32b number \r \n");
value32 = 0;
DebugP_scanf("%d", &value32);
DebugP_log("32b value = %d\r\n", value32);