SPRADL6A January 2025 – January 2025 F29H850TU , F29H859TU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
CCS and VS Code provide a powerful palette of commands that allow users to perform most, if not all, tasks using solely the keyboard. These commands can be activated using CTRL+SHIFT+P. Refer to the table below for some easy-to-use commands enabled by the C2000 IDEA extension. Alternatively, select features have UI buttons available in the C2000 IDEA - Features pane that automatically run the associated commands to activate the feature.
| Purpose | Commands | Devices | Project Detection |
|---|---|---|---|
| Open Tool Walkthrough | C2000: Help Walkthrough | GEN2, GEN3, GEN4 | NOT REQUIRED |
| Run Driverlib Register Vision | C2000: Run Driverlib Register Vision on Current File | GEN3, GEN4 | NOT REQUIRED |
| Run Bitfield Register Vision | C2000: Run Bitfield RegisterVision on Current File | GEN3, GEN4 | NOT REQUIRED |
| Enable Register Coder | C2000: Enable Register Code Write/Read | GEN3, GEN4 | REQUIRED |
| Enable Interrupt Coder | C2000: Enable Interrupt Code Templates | GEN3, GEN4 | REQUIRED |
| Enable Continuous Migration Check | C2000: Enable Continuous Migration Check on Current File | GEN3, GEN4 | REQUIRED |