SPRZ455F December 2020 – February 2025 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
OSPI: OSPI Boot Doesn't Support Some xSPI Modes or xSPI Devices
For background, the various OSPI and xSPI protocols are described according to bit-width (1 or 8) and data rate (S or D for *S*ingle Data rate or *D*ouble Data rate) for the Command/Address/Data segments of the protocol.
The SoC’s ROM OSPI boot mode supports 1S-1S-1S mode and 1S-1S-8S mode.
The xSPI protocol defines 1S-1S-1S mode for general backwards compatibility, and 8D-8D-8D for maximum throughput. The ROM OSPI boot mode is compatible with 1S-1S-1S mode, but is not compatible with 8D-8D-8D mode.
Some SPI Flash memory devices also offer the legacy 1S-1S-8S mode, which is compatible with the ROM OSPI boot mode.
Note that the OSPI IP can in general support 8D-8D-8D mode with an appropriate software driver. The limitation is only for ROM boot which hard codes the 1S-1S-1S and 1S-1S-8S modes.
If 8-bit data rate is required for boot, a SPI Flash memory device should be carefully selected that is compatible with 1S-1S-8S mode of operation.
If 1-bit data is sufficient for boot, an xSPI Flash memory device should be chosen that explicitly supports the 1S-1S-1S mode at boot. Different memory vendors may only support this mode on specific part variants.
TI has identified that Micron’s Xccella OSPI flash is compatible with 1S-1S-8S mode. Cypress Semper Flash does not support 1S-1S-8S mode, and device part numbers should be chosen that explicitly support the 1b boot mode.