SWRA834 May 2025 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Maximum efficiency is obtained by using the internal DC/DC converter, and requires an external inductor and capacitor. Place the components as close as possible to the CC23xx or CC27xx device and have a short current return path from the DC/DC capacitor ground to the pad on the chip. The VDDS pins are not connected together internally. Check the reference design for where each decoupling capacitor needs to be placed. The actual value of decoupling capacitors and the DC/DC inductor can vary from device to device. For the actual values, see the device-specific reference design.
When operating in DC/DC mode, the power system dynamically switches between the Global LDO and DC/DC converter depending on the required load to achieve maximum efficiency. If VDDS drops below 2.2V, then the DC/DC converter is less efficient than the LDO and the device runs in global LDO mode. For systems operating with VDDS less than 2.2V, consider global LDO to save component cost and board area.
To utilize the DC/DC converter, the customer has to select DCDC in the Sysconfig in TI DEVICES -> Device Configuration -> Voltage Regulator. See Figure 9-2 for more details.
Figure 9-2 DC/DC Mode