SWRA834 May   2025 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Reference Designs
    1. 2.1 LP-EM-CC2340R53
    2. 2.2 LP-EM-CC2340R5
    3. 2.3 LP-EM-CC2340R5-Q1
    4. 2.4 LP-EM-CC2340R5-RGE-4x4-IS24
    5. 2.5 LP-EM-CC2745R10-Q1
  6. Schematic
    1. 3.1 Schematic Overview
      1. 3.1.1 48MHz Crystal
      2. 3.1.2 32.768kHz Crystal
      3. 3.1.3 Filter
      4. 3.1.4 Decoupling Capacitors
      5. 3.1.5 Antenna Components
      6. 3.1.6 RF Shield
    2. 3.2 I/O Pins Drive Strength
    3. 3.3 Bootloader Pins
    4. 3.4 Serial Wire Debug (SWD) Pins
  7. PCB Layout
    1. 4.1 Board Stack-Up
    2. 4.2 LC Filter
    3. 4.3 Decoupling Capacitors
    4. 4.4 Placement of Crystal Load Capacitors
    5. 4.5 Current Return Path
    6. 4.6 DC/DC Regulator
    7. 4.7 Antenna Matching Components
    8. 4.8 Transmission Lines
    9. 4.9 Electromagnetic Simulation
  8. Antenna
  9. Crystal Tuning
    1. 6.1 CC23xx and CC27xx Crystal Oscillators
    2. 6.2 Crystal Selection
    3. 6.3 Tuning the LF Crystal Oscillator
    4. 6.4 Tuning the HF Crystal Oscillator
  10. Optimum Load Impedance
  11. PA Table
  12. Power Supply Configuration
    1. 9.1 Introduction to Power Supply
    2. 9.2 DC/DC Converter Mode
    3. 9.3 Global LDO Mode
  13. 10Board Bring-Up
    1. 10.1 Power On
    2. 10.2 RF Test: SmartRF Studio
    3. 10.3 RF Test: Conducted Measurements
      1. 10.3.1 Sensitivity
      2. 10.3.2 Output Power
    4. 10.4 Hardware Troubleshooting
      1. 10.4.1 No Link: RF Settings
      2. 10.4.2 No Link: Frequency Offset
      3. 10.4.3 Poor Link: Antenna
      4. 10.4.4 Bluetooth Low Energy: Device Does Advertising But Cannot Connect
      5. 10.4.5 Poor Sensitivity: Background Noise
      6. 10.4.6 High Sleep Power Consumption
  14. 11Summary
  15. 12References

High Sleep Power Consumption

  • The chip is not going into the lowest power modes when a debugger is connected.
  • Software: Use the gpioshutdown examples in the relevant SDK.
  • When measuring current draw on a Launchpad, remove all jumpers.
  • Make sure that every IC on the board is powered down.
  • If the application is configured to use the 32kHz crystal, then check that this is connected and that the oscillator is running.
  • Make sure no input pins are in tri-state.