SWRA834 May 2025 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Lay out the LC filter so that crosstalk between the shunt components is minimized. Figure 4-2 shows three different layouts from worst to best. The advantage with the layout to the right is that the parasitic inductance in the PCB track (in black) between the shunt capacitor and the series inductor is in series with the inductor. In the middle figure, the parasitic inductance is in series with the shunt capacitor forming a series LC circuit.
If the design cannot use the reference design as-is (for example, use of a different component size), then the filter probably has to be re-tuned. Simulate both the TI reference design and the custom design using an electromagnetic simulator. The two designs have the same S21 and S22.
Figure 4-2 LC Filter PCB Layout Design
Guideline