SWRA834 May 2025 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
The distance from the top layer to the ground layer needs to match the reference design. Deviating from the recommended board stack-up can change the parasitics and, in some cases, can lead to a redesign of the filter. As an example, Figure 4-1 shows the board stack-up, which is used for all CC27xx LaunchPads. The board stack-up for all TI wireless devices can be found in the device-specific reference design.
Figure 4-1 LP-EM-CC2745R10-Q1 Board
Stack-Up