SWRA834 May 2025 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
The CC23xx and CC27xx devices have two crystal oscillators. The high frequency crystal oscillator (HFXT) runs at 48MHz and is mandatory to operate the radio. The low frequency crystal oscillator (LFXT) is used for RTC timing and only required when accurate RTC timing is necessary. For example, synchronous protocols such as Bluetooth Low Energy (see Section 3.1.2).
Both crystal oscillators are pierce type oscillators are shown in Figure 6-1. In this type of oscillator, the crystal and the load capacitors form a pi-filter providing a 180° phase shift to the internal amplifier keeping the oscillator locked at the specified frequency. For this frequency to be correct, the load capacitance must be dimensioned properly based on the capacitive load (CL) parameter of the crystal.
Figure 6-1 Pierce-Type OscillatorA key difference between the oscillators is that the high frequency oscillator has internal variable load capacitance inside the IC and does not require external load capacitors. The low frequency oscillator needs to have external capacitors to operate properly.