SWRA834 May 2025 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
A RF channel receives all radio traffic in the selected frequency span. In addition to the wanted signal, the channel also receives background noise. Part of the background noise is other RF traffic on the selected band. To receive a RF packet, the received signal has to have a given SNR. If the background noise increases, then the practical sensitivity is poorer.
For example, if the conducted sensitivity is -100dBm, the required SNR is 7dB and the background noise is -90dBm, then the practical radiated sensitivity is -83dBm.
Before doing a range test, measure the background noise. One method is to turn off all known TX sources, attach a LaunchPad or a known, good board to SmartRF Studio, select the Continuous RX tab and press play. The average of the resulting graph can be used as an input to find the practical sensitivity.