SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The communication between the host and the network processor uses synchronization words to keep the host and CC31XX device in sync.
There are 2 types of synchronization words in use:
The patterns are given in Table 25-6.
| Sync Word | Pattern (Hex) |
|---|---|
| Host to Device (Long Sync) | 12 34 43 21 BB DD EE FF |
| Device to Host (Short Sync) | AB CD DC BA |
The first 4 bytes of the Long sync are dummy bytes and have no meaning to the CC31XX device. The long sync is required to prevent data loss if the host does not stop the transmission immediately on the next byte when the RTS is raised.