SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The SimpleLink Wi-Fi device offers the ability to predefine specific service types to monitor. If the host application decides not to get responses from certain types of services (not stored in the cache), the adapt bit can be set in the event mask according to the following:
Example:
_i16 Status;
_u32 EventMask;
EventMask = BIT0 | BIT1 | BIT18;
Status = sl_NetAppSet(SL_NETAPP_MDNS_ID, SL_NETAPP_MDNS_QEVETN_MASK_OPT,sizeof(EventMask),&EventMask);
if( Status )
{
/* Error */
}