SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Table 17-3 shows the following values that may be returned when a provisioning command is issued.
| STATUS_OK | 0 | Command was successfully executed. |
| SL_ERROR_WLAN_PROVISIONING_ABORT_ PROVISIONING_ALREADY_STARTED | -2169 | Start provisioning command failed because provisioning process is already running. |
| SL_ERROR_WLAN_PROVISIONING_ABORT_ HTTP_SERVER_DISABLED | -2170 | Start provisioning command failed because the HTTP server is disabled. |
| SL_ERROR_WLAN_PROVISIONING_ABORT_ PROFILE_LIST_FULL | -2171 | Start provisioning command failed because the profile list is full. |
| SL_ERROR_WLAN_PROVISIONING_ABORT_ INVALID_PARAM | -2172 | Start provisioning command failed because one of the parameters was invalid. |
| SL_ERROR_WLAN_PROVISIONING_ABORT_ GENERAL_ABORT | -2173 | Start provisioning command failed because of an unknown reason. |
| SL_ERROR_WLAN_PROVISIONING_CMD_ NOT_EXPECTED | -2177 | Provisioning command failed because it was not expected. |