TIDUF63 December 2023
Input channels can be connected to PV panels and to a 48-V battery. With the PV panel acting as current source, an inrush current is usually not a concern. However, batteries are acting as a very low-impedance voltage source. This means that inrush current can be high and can damage the board.
To limit the current, the following inrush current-limiting circuit was implemented:
When the battery is connected to the input channel - the Q1 MOSFET is turned off. The battery slowly charges the gate of the MOSFET through R61. A Zener diode D3 is used to protect the gate of the MOSFET.