TIDUF63 December 2023
The mission mask for many standards starts at 150 kHz; therefore, selecting a switching frequency below 150 kHz is good design practice. In this design, a switching frequency of 125 kHz was selected for the totem pole DC/AC. By selecting an operating frequency of 125 kHz, the first harmonic does not require significant attenuation but only the successive one as the 2nd, 3rd, and so forth. A current ripple factor of 20 % was selected for the boost inductor, when having 120-VAC output. The inductance value was calculated by using Equation 13 and Equation 14 for a worst-case duty cycle equal to 50%:
An inductance value equal to 106 μH was calculated. Bourns 145450 (D6746) was selected and this is an inductor rated 111 μH. In general, the boost inductor contributes to the differential and common mode noise attention.