TIDUF63 December 2023
The measurement of the AC grid voltage was done using the AMC3330. This device is a precision voltage-sensing reinforced isolated amplifier with integrated DC/DC. This IC has ±1-V input voltage range optimized for voltage measurement with high input impedance. The AC voltage is passed through a voltage divider, thus leading to a linear range of the measurement ±401 V, see Figure 3-14.
The measurement of the DC-link voltage was done with AMC1311, see Figure 3-15. This device is a precision voltage sensing reinforced isolated amplifier without integrated DC/DC. This IC has +2-V input voltage range optimized for voltage measurement with high input impedance. The DC voltage is passed through a voltage divider, thus leading to a linear range of the measurement between 0 V and 441 V. Since the IC does not include a power supply on the high-voltage side, the GaN power supply was used for this purpose.
The measurement of the DC-link current was done with AMC1302. This device is a precision current sensing reinforced isolated amplifier without integrated DC/DC. This IC has +50-mV input voltage range optimized for current measurement with low input impedance. The DC current is passed through a 2-mΩ shunt, thus leading to a linear range of the measurement ±25 A.
The current in the grid is measured by means of a Hall-based current sensor TMCS1123 which allows measurement of the current into the Point of Common Coupling (PCC) with high accuracy. This design allows a reinforced isolation between the grid and the MCU.