TIDUFB1 December 2024
In this build, the board is operated as a three-wire system, that is, the neutral of the power supply is not connected to the DC midpoint of the output. As Figure 3-28 illustrates, to maintain the DC bus balance, a balance loop with a simple proportional gain is added in the control structure. In this build a third harmonic injection is also carried out, which helps in stabilizing the DC bus balance point.
Figure 3-28 Build Level 4 Control Diagram:
Output Voltage, Inductor Current, and Bus Cap Balance Loop