TIDUFB1 December 2024
Figure 3-46 , Figure 3-47, and Figure 3-48 show voltage short interrupt tests under 5kW at 90, 0, and 45 phase angles. The current on boost inductors is monitored by DSP internal CMPSS, if this current is too big, IGBT is turned off on each PWM cycle. This is the cycle-by-cycle protection. However, DSP cannot protect current on diode bridges, since there is still uncontrolled rectified current with diode bridges when IGBTs are off.