TIDUFB1 December 2024
First a virtual neutral is constructed by using a resistor network connected in Y along with some capacitance for stability. In this design, the controller is kept on the cold side, thus, an isolated amplifier AMC1350 is used to process the VL-N’ voltages as shown in Figure 2-8. As the AMC1350 is designed considering low-impedance sources for current-sensing applications, the input differential resistance plays a non-linear role in the total gain calculation. Therefore, a final calibration during build level one must be done, and the maximum AC voltage range must be adjusted according to the calibration.
Figure 2-8 Input AC Voltage Sensing