TIDUFB1 December 2024
The bus capacitor is responsible for removing the ripple on the DC voltage that can be caused by the draw of sinusoidal currents. The capacitor value and the DC bus ripple are related by Equation 12.
This equation is used to select the minimum DC bus capacitance value.
The calculation in Equation 12 can yield to an over design of the capacitor. The capacitor sizing is more dependent on the load and the nature of current drawn. For three-phase PFC the power ripple is fairly small as the input always has a path to the output. Only use Equation 12 for reference and be aware that this yields to over design.