TIDUFD2 May 2025
PV micro inverters require an isolation between PV panels and the AC grid because of a variety of reasons, such as the following:
From a safety point of view, micro inverters combined with PV panels are commonly installed by the end-user, thus reinforced isolation between the panel and grid side is required to mitigate the electrical shock hazard from AC grid side.
The common-mode currents are a well-known challenge in PV applications due to PV surfaces exposed over grounded roofs or other surfaces in the proximity. This enormous quantity of surface leads to high parasitic capacitance between the panels and the ground (up to 200nF/kW). This parasitic capacitance can cause high common-mode current flowing into the system when common-mode voltage of the converters is not mitigated enough. A common strategy to significantly reduce the parasitic currents flowing in the system is using an isolation stage between the panels and the grid.